Hi,
I need to translate 3V logic signals to an equivalent higher voltage signal, where the Voh and Vol can be set to -2V and 15V for example.
Ideally, I would like to be able to set the VOL and VOH to lie anywhere in the range from -15V to +15V, but obviously where VOH>VOL.
Here are some examples;
VOL=1V, VOH=3V
VOL=0V, VOH=6V
VOL=-1V, VOH=15V
VOL=-2V, VOH=6V
I can use a translator device or individual op-amps. Any appropriate device for this purpose?