I have ADS4229 Evaluation board. ADS4229 which has outputs are at 1.8V. I am using SN74AVC16T245 to convert +1.8V to 3.3V. Sampling rate of ADC is 245.76 MHz. Clock (sinewave)which is output from ADC (clockout) as input to SN74AVC16T245 to convert it to 3.3V.
When input clock frequency or sampling rate is less than 150 MHz it is working fine. When input clock frequency is 245.76 MHz, clockout from ADC is fine but output of SN74AVC16T245 is distorted.
So what is maximum frequency as input can be used with SN74AVC16T245 ?
What are other solutions I can used if SN74AVC16T245 not able to handle frequency higher that 150 MHz ?
Thanks.