Hi TI support and folks,
I plan to use a 3 input OR gate, the SN74LVC1G332. It would be powered by a battery so the expected supply voltage could be from 3.5V to 4.2V. One of the inputs would be of 2.85V level.
The datasheet of SN74LVC1G332 shows the high-level input voltage thresholds over different power supply ranges. However, the threshold for power supply between 3.6V to 4.5V is not provided. - There are some gaps over the entire voltage supply range.
Can someone provide the high-level input voltage threshold of SN74LVC1G332 for power supply between 3.6V to 4.2V?
Thanks.
Best regards,
Frank