Hi guys, I need your help ASAP, since I am already in layout stage. I connect TMS320C6415 to pci connector through SN74CBT16211A bus switch in order not to damage the DSP processor when I connect it to 5V I/O environment. Doing that I violate the PCI spec. line lengths. I mean the clock line is not 2.5 inches long and the AD lines are longer then 1.5 Inches since they go through the bus switch. (I use 33 MHZ - 32 bit PCI spec). 1. How SN74CBT16211A will affect the line lengths? 2. Is the line length is important for the non terminated bus architecture? 3. Can you think of Ideas?
Thanks!!!
Happy Holidays!!!