This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4504B not working when Vcc = 0V ??

Other Parts Discussed in Thread: CD4504B

Dear Experts,

I'm using a CD4504B level shifter to translate 5V signals to 12V.
However, the 5V power supply is not always present...
... and I have the impression that the device is doing stupid things (high power consumption, and output switching unexpectedly (at least it happened once...)).

Inputs are also not powered, but I have pull-downs on all the inputs, so I presume they should not disturb the CD4504B, but I can find no information about what is supposed to happen when VCC = 0 and VDD = 12V...

Does anyone know?

Thanks for your help!