Is there a maximum negative voltage range for SN74LVC1G332 (or similar logic gates)?
I got +/- 5V from a window comparator (-5V should be low) but there is no information in the datasheet about what happens if there is a -5V Input voltage.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a maximum negative voltage range for SN74LVC1G332 (or similar logic gates)?
I got +/- 5V from a window comparator (-5V should be low) but there is no information in the datasheet about what happens if there is a -5V Input voltage.
The recommended operating conditions in the SN74LVC1G332 datasheet suggest an input voltage between 0 V and 5.5 V. The part will become damaged from any input voltage outside of the absolute maximum range, -0.5 to 6.5 V.