This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[ SN74LS244 ] Terminate Unused Input to Different Voltage

Other Parts Discussed in Thread: SN74LS244, SN74LVC244A

[ SN74LS244 ] Terminate Unused Input to Different Voltage

Hi Expert,

I understand that it should be prevented to leave unused input pin open (floating) for CMOS input, and it's suggested to connect either Vcc or GND.

However, what about connecting to the different voltage than Vcc?
As indicated in the drawing below, SN74LS244 is powered with 5V, however, unused input is connected to 3.3V via a resistor.

Can we recommend this connect?

Thanks,
Ken

"Must-Check" FAQ before posting...
Floating the inputs of Logic devices
e2e.ti.com/.../2945.floating-the-inputs-of-logic-devices