Other Parts Discussed in Thread: SN74HC595B
Dear Specialists,
My customer is designing SN74HC595B, and he has some questions.
Could you please advise them.
(1) where should be connected? The datasheet is not described.
Generally, exposed pad is connect to GND.
How is this device? Can he consider similarly?
(2) What is the maxmum frequency at 3.3V supply?
The datadheet say only 2.5V, 4V and 6V, not 3.3V
My image, should he be calculated by 5MHz@2.5V and 25MHz@4V.
In this case, 15.23MHz@3.3V, is it correct?
(3)connection for not using pin, OE, Qh' and SRCLR.
Are they correct for not using
OE:GND directly connect
Qh':OPEN
SRCLR:3.3V directly connect
I appreciate your great help.
Best regards,
Shinichi