This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHC1G04: SN74AHC1G04DCKR - The variability of output resistance

Part Number: SN74AHC1G04

Hello,
I have a request about SN74AHC1G04.

Is there the following data?
・The variability of output resistance.
  For example, 70Ω(High) 45Ω(Low) @25℃
or
・Vo (output voltage) vs Io (output current)  High and Low

[supplementary explanation]
In brief, for a 1mA load, I want to know how output voltage variability turns out.
I OK even it if I understand output resistance (I calculate in I*R).
Or by the specification of Vo vs Io, I can estimate output Z equally.

Regards,
Dice-K