Other Parts Discussed in Thread: CD74HC4316
Hello,
I understand from reading datasheet that the amplitude of the input signals must be in the power rails range (0 to +5V in this case) to pass through this switch. I have an application where the input signal can be negative as it is an error signal out of comparing two signals. What is the best solution to handle the negative input voltage with this switch? Are there similar switches with -5V to +5V power rails?
Thank you in advance,
Sanaz