This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC132-Q1: Temperature-Compensated Threshold Levels

Part Number: SN74HC132-Q1
Other Parts Discussed in Thread: SN74LVC1G132

Dear Team,

we received a request regarding the threshold level of our logic device SN74HC132-Q1. The customer wants to use the device at 5V and 3.3V.

The datasheet mentions the threshold level with min/max values as well with a typical value @ 25°C.
The complete temperature range only states min/max values.

Since the part has temperature-compensated threshold levels:

Is the assumption correct, that the typ. threshold level stays the same over the complete temperature range?
And the part-to-part variation is within the min/max values?

Thank you for your support!

Best Regards
Martin