This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV06A: Low level(Vol) data

Part Number: SN74LV06A

Hi,

I would like to ask you a max Vol (max low level output) data in case following conditions.

  - Vcc = 5.0V

  - Iol = 6.25mA(min) to 10mA(max) 

 Do you have the data of Vol?

Because there are some data under some conditions at datasheet page5, 6.5 section as below.

I suppose the max Vol seems to be lower than 0.55V at Icl=10mA/Vcc=5.0V according to this table.

But if you have more information/data, please let me know.

Thank you for your support.

Best Regards,