This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHCT1G08: Required VIH & VIL values for SN74AHCT1G08 at TA = –40°C to 125°C.

Part Number: SN74AHCT1G08

We will use SN74AHCT1G08 single 2-Input Positive-AND Gate. In our system, input voltage is maximum 3.3V . In a datasheet, the Recommended Operating condition for  VIH(min)=2V & VIL(Max)=0.8V.

I would like to know the DC electrical charactristics for the VIH & VIL values. Please can you provide me the details (VIH & VIL)  for the TA = –40°C to 125°C.

  • Hello Kedar,

    VIH and VIL are recommended specifications for a good reason - there is no electrical specification for them.

    Using VIH as an example, if your input voltage is larger than or equal to VIH, then you are guaranteed from TI that the device will recognize that signal as a logic 'HIGH.' If your signal is below that value, we cannot guarantee that the input will recognize the signal as a 'HIGH.'

    Physically, the device will transition from a LOW input to a HIGH input somewhere around VCC/2, which is called the 'threshold voltage,' or VT in datasheets. You will note that we don't specify VT for standard CMOS devices -- this value isn't particularly useful in operation since the input should be transitioning from LOW to HIGH in just a few nanoseconds, and the threshold value is inconsequential for the ouput timing when operating the device appropriately.

    If you need a device that can support slow inputs, or one that has a well defined threshold voltage, those are two different devices -- for slow inputs, use a Schmitt-trigger input logic device.  For a specific threshold voltage, use a comparator.