In Logic Guide by TI,attached,5V TTL and 3.3V LVTTL trigger voltage is 1.5V.Can you explain why?And WHY CMOS trigger voltage is 1/2 VCC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In Logic Guide by TI,attached,5V TTL and 3.3V LVTTL trigger voltage is 1.5V.Can you explain why?And WHY CMOS trigger voltage is 1/2 VCC?
The switching threshold is designed so that you get the largest possible noise margin.
For (LV)TTL, VOL = 0.4 V and VOH = 2.4 V, so the threshold is in the middle of this interval (1.4 V) so that you get 1 V noise margin in both directions. (The actual threshold depends on VCC and might have hysteresis, so it's near both 1.4 V and 1.5 V; see below.)
For CMOS, VOL and VOH are symmetrical, so the middle of the VOL/VOH interval always is half of VCC.