This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

74ACT16244: Clamp diode Voltage Level Arrange

Part Number: 74ACT16244


Hi Logic team

Part number : 5962-9202201MXA (SNJ54ACT16244WD)

                       16Bit Buffer/Line Driver with 3-state Outputs

Can I get information which is Clamp diode Voltage Level as a red box below.

Best Regard

Gerald

  • Gerald,
    This can be inferred from the absolute maximum rating entries for VI.
    In this case, the entry is -0.5V to VCC+0.5V. This indicates that both the diode to ground and VCC will start conducting around 500mv above VCC and below ground.
    Regards,
    Wade
  • Hi Wade

    Thank you for your reply.

    1. Can we get information Which is Clamp diode Voltage at the AHC and HD of TI Logic family as a picture above ?
    2. Can we get information and document Derating grahp each temperature(example -40C, 25C, 70C, 125C)

    If you have any question contact me anytime.

    Best Regards
    Gerald