Hi,
I want to add pull up resistor in the input side for 5volt.
Can you please help me to select a pull up resistor value limit?
Thank you in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to add pull up resistor in the input side for 5volt.
Can you please help me to select a pull up resistor value limit?
Thank you in advance.
The datasheet mentions a theoretical maximum leakage current of 20 µA, so to prevent the voltage drop over the resistor from becoming too large, it must be less than 85 kΩ. (See Choosing an Appropriate Pull-up/Pull-down Resistor (SLVA485).)
If the pull-up resistor is only a fallback for when the actual signal source is not present or not yet powered up, then you don't need to go lower. Use a common value like 68 kΩ or 47 kΩ.
But if you are using an open-drain output to drive the signals, then it might be necessary to use a lower value, depending on what frequency you need to achieve.