Other Parts Discussed in Thread: TXB0108, TXS0108E, SN74LVC2T45, SN74AVC2T45, LSF0108
How do you calculate the pull up resistors for the SREF port when the input voltage can vary from 1.2V to 3.3V, form an FPGA module source. And the DREF port is a fixed voltage of 3.3V. The DREF resistors are easily calculated. However for the SREF do you design for the 3.3V potential voltage, and then the lower voltages are covered?