Hi
Our customer are considering the damping resistor. If the Pin#4(output of channel 2) is connected to Pin#1(input of channel 1), should we add the dumping resistor between Pin#4 and Pin#1?
I think the pattern trace is very short and does not need. (signal freq:120kHz. the trace is connected as possible as short.)
Regards,
Koji Hamamoto