This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LS628: Connection of RX pin

Guru 16770 points
Part Number: SN74LS628


Hi

1.

Could you check the following connection of RX pin?

Is it correct?

2.

Is it possible to use other than 600ohm?

If yes, what is the impact of changing resistor value?

BestRegards