Dear all,
in the document SCEA002A, there is an overview of the LVT family: in figure 13 and in figure 14 the rise time and fall time vs. temperature is showed.
Both rise and fall time have value less than 2ns, which are good for the requirements of the application of my AA customer.
Unfortunately I cannot find any DS of the the LVT family which shows that value. In most of the case the rise time has just a spec as max value (10ns).
Were the values in the SCEA002A just typical ? If not can you indicate a buffer, 3.3V which has a Trise comparable wih the one showed int the SCEA002A ?
regards,
Domenico