Other Parts Discussed in Thread: SN74LV1T08
Hello,
I’m trying to determine the typical and max supply current draw that the SN74LV1T34 part needs. Page 3 of the datasheet says that worst case (per chip) continuous supply current is 50mA.
- What is the worst case current for non-continuous?
- And why is this listed as +/-50mA when this is a single supply part?
- Page 5 of the datasheet shows a no-load supply current max of 10uA. It then specifies a ‘delta’ supply current max of 1.5mA (under certain circumstances but no output current).
- Why does this supply current specification talk about ‘one input’ and ‘other inputs’ when this is a single input device?
- What does ‘delta’ supply current mean in this context? Does it mean that you add 1.5mA for each shift condition?
- What is the worst case supply current (for Vcc = 5V, at full high and low level output current) for any level shifting configuration?