Hi,
I'm looking at the SN74AVCH4T245 datasheet and have a few questions:
- Datasheet states the outputs are disabled to prevent damaging current backflow when the device is powered down.
- Is this independent of the the Direction pins are set to? In other words, are ALL I/Os put into high impedance states regardless of whether the pins are set to inputs or outputs?
- The Ioff spec shows that both VCCA and VCCB can be 0V and the outputs will still be disabled.
- Why is the terminology of "Partial-Power-Down Mode" used? Why would it not be just "Power-Down Mode" if no voltage is supplied to either power rail?
- Basically, I just need to ensure that when no voltage is supplied to the chip, if the inputs of the chip are driven, is back-power prevented in all cases as long as OE pin is tied to VCC via resistor?
Thank you!