The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC8T245: Will SN74LVC8T245 and sn74AHCT1G08 be damaged during hot plug? --Urgent!

Part Number: SN74LVC8T245
Other Parts Discussed in Thread: SN74AHCT1G08

Hi Team,

My customer is trying to use SN74LVC8T245 and sn74AHCT1G08 in the new project to connected to backplane board directly without protection, they have question that if SN74LVC8T245 and sn74AHCT1G08 will not be damaged during hot plug? If not, do we have solution to avoid damage during hot plug? As they need to send out the pcb very soon, need your kindly support to check this.

Thanks for your support. Below are their schematic:

Can you help check and give solution if SN74LVC8T245 and sn74AHCT1G08 can't handle directly, thanks a lot!

  • Hi Sulyn,
    I see that there is external ESD protection, which is very good.

    As long as the ground connection is made first, then Vcc, followed by any signal lines, the devices won't be damaged.

    These devices aren't rated for hot plug applications, so the data bus they are connected to could become corrupted during plug-in. If that's not a problem, then the system should be fine as shown. There's an application report that discusses the levels of hot-insertion capability located here: www.ti.com/.../scea026.pdf