Other Parts Discussed in Thread: SN74LVC1T45
Hello,
What is the drive strength of the TXS0101YZP? The source current of the driver is 10mA. Can i use this for the driver whose drive strength is 10mA?
Thanks,
Louie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What is the drive strength of the TXS0101YZP? The source current of the driver is 10mA. Can i use this for the driver whose drive strength is 10mA?
Thanks,
Louie
Hi Louie,
The TXS0101 is a fairly complex device including both active and passive translation elements. It includes one-shots that drive the outputs for a very brief period of time when a rising edge is seen on the opposite pin, but otherwise the drive strength comes from the driver (for sink current) or the pull-up resistor (for source current).
Please forgive my artwork. If a driver is forcing pin A low, then the current will sink from B to A into the driver. If the driver is forcing pin A high, then the center switch will be in 'high impedance' mode, and the output current will come through the pull-up resistor.
For a very brief period of time, the one-shot will bypass the pull-up resistor to help pull the line high faster, but then it turns off and the line is held by the 10kohm resistor.