This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV07A: VOH at different load conditions

Part Number: SN74LV07A


Hello Team,

In SN74LV07A datasheet page 5, there are VOL at different load test conditions. May I know if VOH specs are the same with VOL at different loads? For instance, in conditions of Iout 16mA, -40C to 125C, VOL max is 0.55V, and VOH min is VCC - 0.55V?

Regards,

Ting