This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G08: the temperature and power consumption

Part Number: SN74LVC1G08


Hi 

My desing is VCC=5V , and driving around 30mA (LED)

is that mean power consumption is 150mW , and DBV package will increase 206x0.15=30 

thanks