Hello, I don't understand Luke Sun's answer (Dec 5, 2016 3:18 PM) about 10MHZ SPI with SN74LVC157A.
Dennis said that we can use propagation delay to estimate maximal frequency:
With VCC=3.3V:
2x5.2=10.ns
fmax=1/10.4ns~96MHz
With VCC=1.8V:
2x14=28ns
fmax=1/28ns~35.7MHz
In all cases, this frequency is much greater than the frequency of 10MHZ of SPI.
So why Luke wrote "Then SN74LVC157A seems couldn't support 10MHz SPI".
Have you got a specification of maximal speed of 74lvc157A gate?
Regards.
Sylvain