Other Parts Discussed in Thread: SN74LVCH8T245
Hello,
For new FPGA technologies such as Intel ARRIA10, it is recommended to operate FPGA-IOs in a 3.0 V environment.
Are there solutions for connecting a medium size parallel bus system to such 3V FPGAs.
Up to now we use the 74LVTH245 (which is able to drive low Level currents of 64mA@0.55V ) for interfacing it to an 3.3V FPGA
For a new ARRIA 10 design we need to rework the Interfaces.
It would be nice to find a Dual Supply / Direction controlled Level Translator like the 74LVTH2240WM with higher current driving capabilities on the market.
There is no Chance to drive a medium size bus system with IOL max 12mA (from 74LVTH2240WM data sheet) .
Are there any plans from TI or ideas to match this requirement ?