Other Parts Discussed in Thread: TXB0104
I am using the TXS0104ERGYR BIDIRECTIONAL translator. One side Vcca = 1.8V (driven as a GPIO pin from a iMX7 processor), other side of TXS part is 3.3V for local devices.
The Voh (min) from iMX7 is 1.44V.
The Vih (min) to TXS part is "Vcca - 0.2V" = 1.6V. I am worried this may cause a "high" from the iMX7 not be pass thru the translator. See data sheet 6.3 Recommended Operating Condition".
I am surprised that the TXS part requires Vih just 0.2V from the 1.8V rail - Is this correct? How can I correct this? I have looked at other TI parts, - I do not want to look at other voltage translation parts that require external pull-up on each I/O pins.
Thanks
Buck Patel