This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1T57: Difference between SN74AUP1T57/58/97/98

Part Number: SN74AUP1T57

Hi Team, 

I saw voltage level device SN74AUP1T57 / 58 / 97 / 98, according to datasheets, they are same? so it's just generation difference? which means I should recommand customer the latest one N74AUP1T98?

Thanks a lot.

Yang

  • Hello and thanks for your post! Today is a holiday in the US. I just wanted to let you know that we will get back to you on Monday, November 26.
  • These four devices are all different:

    Use whichever one that implements the desired logic function(s):

    57

    2-input AND gate
    2-input NOR gate with both inputs inverted
    2-input NAND gate with inverted input
    2-input OR gate with inverted input
    2-input AND gate with both inputs inverted
    2-input NOR gate
    2-input XNOR gate
    Inverter
    Noninverted buffer

    58

    2-input NAND gate
    2-input OR gate with both inputs inverted
    2-input AND gate with inverted input
    2-input NOR gate with inverted input
    2-input NAND gate with both inputs inverted
    2-input OR gate
    2-input XOR gate
    Inverter
    Noninverted buffer

    97

    2-to-1 data selector
    2-input AND gate
    2-input OR gate with one inverted input
    2-input NAND gate with one inverted input
    2-input AND gate with one inverted input
    2-input NOR gate with one inverted input
    2-input OR gate
    Inverter
    Noninverted buffer

    98

    2-to-1 data selector with inverted output
    2-input NAND gate
    2-input NOR gate with one inverted input
    2-input NAND gate with one inverted input
    2-input NAND gate with one inverted input
    2-input NOR gate with one inverted input
    2-input NOR gate
    Inverter
    Noninverted buffer