This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVTH125: Thermal information not in datasheets

Part Number: SN74LVTH125
Other Parts Discussed in Thread: SN74CB3T3245, SN74LV4T125

 Hi guys,

Can you help me find the below info for these logic devices? We can't find them in the datahseet.

Junction-to-Ambient Thermal Resistance

Junction-to-Case (top) Thermal Resistance

Junction-to-Board Thermal Resistance

Max Junction Temp

Min Junction Temp

XES P/N

TI Part Number

Description

RƟJA [°C/W]

RƟJC [°C/W]

RƟJB [°C/W]

TJ,max [°C]

TJ,min [°C]

40000086

SN74LVTH125RGYR

IC, Quadruple Bus Buffer, SN74LVTH125, QFN-14, IND

 

 

 

 

 

40000057

SN74LVTH125PWR

IC, Quadruple Bus Buffer, SN74LVTH125, TSSOP-14, IND

113

 

 

 

 

40003245

SN74CB3T3245DGVR

IC, 8-Bit FET Bus Switch, SN74CB3T3245, TVSOP-20

92

 

 

150

 

Thanks,

Brian