Other Parts Discussed in Thread: SN74AXC1T45
Dear TI
I have a follow up question to my question in this post.
Consider the following situation: Vcc is 0 V, the output-enable OE is at logic high (1.8 V) and the line connected to the output Y is at 2 V.
Will the output then be at high-impedance and sink no current or does the OE feature not work if Vcc is 0 V and the output will sink some current? If yes, how many μA may this be?
The background is:
We are trying to minimize the current used by the SN74LV1T125 if the device is not in use but there is a voltage of 2 V at the output. Would it be best to keep the supply voltage at 3.3 V and pull OE to high?
Thank you and best regards
Thomas