This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G123: SN74LVC1G123

Part Number: SN74LVC1G123


Hi Sir,

I am planning to use the part SN74LVC1G123 as per given configuration. Can you review the diagram and share your comments.

Regards

Anuraj NK

 

  • Hi Anuraj,

    I would recommend either using the "B" input or the "CLR\" input rather than tying both together.

    Note the difference in function -- the CLR\ pin forces the external capacitor to charge while it is LOW, producing a sharp edge and a nearly instant reset of the RC timing circuit (also cutting the output short).  The A\ or B signals will only have an effect on the timing circuit when the appropriate edge is detected. As you can see here, A\ goes HIGH and the charging waveform is not affected -- until A\ goes LOW, triggering an output pulse. The B input works the same -- if it is driven LOW, the output will not change, but when it goes HIGH an output pulse is triggered.

    If this answers your question, please click the green "this resolves my issue" button - if not, please respond and I will continue to help.