This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV1T08: Are the inputs loaded if the device is not powered?

Part Number: SN74LV1T08
Other Parts Discussed in Thread: 2N7001T

I am looking to use a SN74LV1T08 as a voltage translator between 1.8 V on the input and 3.3 V on the output.  It is likely that at some point the input signals will be active while the output voltage domain is off.  Will there be a load on the input if they are driven high into the part while its power is off?