This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

14-24-LOGIC-EVM: leakage current

Part Number: 14-24-LOGIC-EVM

The pin 1 of CD4071BE through a 10KOHM is connected to "0" gives me 1.44v on pin 1.  The measured leakage current to "0" is 120uA. With a 47KOHM pull down resistor on pin one the output stays high at 3.78V.

CD4071BEs are purchased from Digikey and 4 of them are tested that give same results.

The leakage current doesn't match with the spec SCHS056D  that it should be less than 0.25uA.