Hello,
I am using the LSF0204-Q1 Levelshifter in my application.
1) Can the channels be operated independently in different directions at the same time (for example channel 1 from A to B and at the same time channel 2 from B to A)?
2) Could i use on VREF_A any voltage between (0.95 V - 3.3 V ) and translate it to any voltage on VREF_B (1.8 V - 5.5 V) ? (for example VREF_A 1.65 V to VREF_B 3.3 V)
Thanks in Advance.
Mohammad