This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G14-EP: Over-Voltage Tolerance Inputs

Part Number: SN74LVC1G14-EP

Hello,

We are considering SN74LVC1G14-EP component as our Schitt-Trigger Inverter.

Here is the example we would like to show the example reagarding over-voltage tolerance inputs.

eg: Supply Voltage Vcc = 3.3V

      Input Voltage Vi = 5V

Does the condition stated above would impact the function and performance of the SN74LVC1G14-EP?

Will the condition above be harmful for SN74LVC1G14-EP?

We are looking forward for the response.

Thank you!

-Hasif