This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G14: what's the Iq of SN74LVC1G14 at VCC=5V, A=2.6V?

Part Number: SN74LVC1G14
Other Parts Discussed in Thread: SN74LVC1T45

Hi

customer want to know what's the Iq of SN74LVC1G14 at VCC=5V, A=2.6V?

thanks.

  • Hi Max,

    Is there a reason why 2.6V input is used? The output is not guaranteed to switch at Vcc 5V and input at 2.6V.
    The Icc can be very high in mA during this case and could cause reliability issues in the long run.

    Consider using a voltage level translator with Vcca at 2.5V and Vccb at 5.5V like SN74LVC1T45.