This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4555B: What are the Logic Levels, if the supply is 3V3?

Part Number: CD4555B


Hello,

The datasheet states the part can be supplied from Vdd=3...18V

The characteristics are based on the conditions Vdd=5V/10V/15V.

- Applying Vdd=3.3V, having other 3.3V logic components on the circuit,

  What are the threshold values for the inputs and outputs?

Thanks.