The circuit is now designed with SN74ABT245BDGVR parts.
1. Input signal : 5V level
2. Output signal : 3.3V level
3. Operating voltage : 3.3V
Since it is designed differently from the operating voltage on the datasheet, I want to change SN74ABT245BDGVR to SN74LVC245ADGVR.
So I want to use the SN74LVC245ADGVR to determine if the circuit configuration is suitable.
Also let me know the percentage of defective parts SN74ABT245BDGVR in use.