Team,
My customer is observing behavior that contradicts datasheet:
The datasheet for the LM567C states that the “device is designed to provide a transistor switch to ground output when the input signal matches the center frequency”. I have a device hooked up with a microphone and preamp as an input and my output is showing a low until I turn on the tone generator and then it switches high. As I read the datasheet this is reverse from the description as well as the example waveform shown. My first thought was that there was sufficient ambient noise to give me a true reading, but after turning on my tone generator and seeing the output switch it leads me to believe I’m getting a reverse behavior. Is there something I’m missing here?
Thanks!
Viktorija