This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS26LV31QML Line driver Logic high and low output voltage

Part Number: DS26LV31QML

Hi;

what is the output high and output low voltage (Voh Vol) of DS26LV31QML line driver and give the test condition to measure the same

Thanks

Midhun

  • Midhun,

    The datasheet specifies the differential Vod output voltage.  The VOL/VOH are not defined, as the device is intended to be used as a differential driver.  Vol/Voh are single ended parameters.

    The output Vod is defined with several test conditions in the DS using 100 ohms, and 3900 ohms across VCC range.

    If this answers your question, please click "This Resolved My Issue"
    Regards,
    Wade