This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHCT14: If the datasheet doesn't indicate delta ICC parameter, do I need to worry about the current spike?

Part Number: SN74AHCT14
Other Parts Discussed in Thread: AM26C32

Lets say if it is a line receiver, in the case that all the inputs are not in the rail in some situation. 

here is the paragraph from ahct14 datasheet

7.9 Typical Characteristics One common misconception is that the current consumption will be less when switching a slow signal into a Schmitt trigger. This is partly true because the Schmitt trigger prevents oscillation which can draw a lot of current; however, you will see higher ICC current due to the amount of time the input is not at the rail. This is Delta ICC. Delta ICC is where the inputs are not at the rails and upper or lower drive transistors are partially on. Figure 1 shows ICC across the input voltage sweep.

thank you so much in advance!!