Part Number: SN74LVC1G3208
Hi team,
If we apply 3.3V to VCC, and add pull up resistor on the output, Y, it there any risk to such application?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC1G3208
Hi team,
If we apply 3.3V to VCC, and add pull up resistor on the output, Y, it there any risk to such application?
Hi Charles,
What are you pulling the output up to? Whats the value of the pullup? If it's to VCC then there won't really be any issue unless its a very strong pull-up. The device will need to be able to sink the current during a Low output.
Hi Dyland,
Thank you for your help here. I have missed some word here, the Y will pull up to 5V with 4.7k ohm resistor. Will it be a problem? Thanks.
Hi Charles,
4.7kohm will be large enough to limit the current to avoid damage of the device, but when the device outputs a High there will be current flowing back into the 3.3 V supply.