Part Number: SN74HC02-Q1
What is the input and output drive configuration (CMOS/ Pushpull CMOS) of "SN74HC02-Q1" logic gate? and What is the drain to source ON resistance of CMOS configuration (Input and Output)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74HC02-Q1
What is the input and output drive configuration (CMOS/ Pushpull CMOS) of "SN74HC02-Q1" logic gate? and What is the drain to source ON resistance of CMOS configuration (Input and Output)?
Everything is CMOS; see HCMOS Design Considerations.
The worst-case output impedance can be computed from the VOL/VOH specifications in the datasheet: 0.4 V / 5.2 mA ≈ 77 Ω (at VCC = 6 V).
The inputs are connected to the gates, so the input impedance is approximately inifinite.
You could also consider the newly released HCS family of devices and is P2P with the HC02-Q1.