Other Parts Discussed in Thread: SN74LVC244A, SN74AUP1G17, SN74AUC1G17, SN74AXC1T45
Dear all:
Unfortunately, I don't have so much experience with logic yet. That's why a have a fundamental question regarding
Buffers and their capability to drive Termination resistors.
I got some digital singnals with up to 150MHz and 3,3V Level coming from a relatively weak Driver
over a cable to my PCB. Then, I need to place some long PCB tracks with 30-50cm of length using several vias.
So I need to use Buffers to recycle my Signals, (Eg. the SN74ALVCH244PWR or SN74ALVCH16827DGGR)
and especially after this long pcb trace length I need to use a proper Termination.
Unfortunately all of these Buffers are not very strong (24mA DC per Channel @3V if I understand correctly), so my idea is
to set the impedance matching of my PCB tracks to 120 Ohm and terminate all Signals with 240Ohm to my Supply (3,3V)
and 240 Ohm to GND (=Thevenin Termination, =120Ohm AC Resistance). I thought, that the mentioned Buffers can drive this load.
To ensure this is working I did small test: I put a SN74ALVCH244PWR on a PCB and directly put this kind of termination
on its Output while driving a 100MHz-Signal. Using a active Probe I measured the Signal and it doesn't look good.
The Signal is rather a Sine wave and is lifted of the GND. So the Driver seems to be to weak to drive this.
Can you give me a hint on what I'm doing wrong? Am I using the wrong devices? Or is there generally a better way to do this?
What I understood so far is that my source Signal also doesn't look very good when arriving at my pcb connector,
and that's why I need to use a better connector and a Buffer with a Schmitt Trigger Input at my first Input Stage (of my PCB).
Hint: I'm doing a test PCB. Cost and PCB space is not critical.
Thanks in Advance!!