This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DGV package for part number SN74AVC16T245DGVR

Other Parts Discussed in Thread: SN74AVC16T245, SN74AXC8T245

the datasheet for SN74AVC16T245DGVR lists DGV as one of three different options. 

DGG

DGV

BGA MICROSTAR JUNIOR. (life buy)

while the datasheet lists these 3 options, the drawing and or footprint information is missing for DGV.  so.. which drawing should i use when makeing a footprint for SN74AVC16T245DGVR?

thanks

  • I also wanted to say.. 

    discontinuing the BGA MICROSTAR JUNIOR package is causing me quite a bit of .. pain.. I have this package designed in to a couple of products. the reason for using that package is nothing else would fit. now I am having to do a redesign to fit the much bigger DGV or DGG packages. is there something i am missing or is there another product that fits in the same space as  SN74AVC16T245 with the BGA MICROSTAR JUNIOR package?

    thanks

  • Hi Ron,

    This link will show the device dimensions, not sure why its not showing up in the datasheet, but I will add this to our queue to get fixed.

    Unfortunately, we can no longer support the microstar package, but we do have a better suggestion for reducing size compared to using the DGG or DGV package. If you use two SN74AXC8T245 devices in either the RHL or RJW you will save space and it will provide the additional benefits that come along with our new AXC family.