This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4027B: CD4027B: The otput Q won't change UPDATE

Part Number: CD4027B
Other Parts Discussed in Thread: CD4016B, , TS12A4514, CD4066B

Dear * all,

i changed the input buffer form  CD4050B for a CD40106B so i connected

-> button from Pin1 ( CD4016B) to gnd, and added a 100k pull-up to 12V from Pin1 ( CD4016B)

-> when i press the button Pin2( CD4016B) goes UP ( this works ok)

-> then i connected J2 and K2 from CD4027BE to 12V, Set2 and Reset2 to GND .

-> and finaly i connected the PIN2 (CD4016B) direct to PIN3 (CD4027BE)

and now the Q2 and !Q2 stay after input change in they state.

But sometimes after  button press the output Q won't change?

1) do i need an RC IN pin1 of CD4016B?

2) do i need a pull-down on pin3 CD4027B?

3) do i need a RC on pin3 CD4027B?

[ i currently don't have access to a scope ]

Best Regards.