This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1T34: Down Shifting Possible?

Part Number: SN74AUP1T34
Other Parts Discussed in Thread: 2N7001T

Hello,

I was wondering if this part would allow you to go down in voltage as well as up.  The datasheet only mentions going up in voltage and I would like to go down to 1.8V from 3.3V.

Thanks,

Robert

  • Hi Robert,

    Yes, this device can do up and down level translation depending on the output Vcc voltage level.

    In your case, the Vcca = 3.3V and Vccb = 1.8V.

    You could also consider using 2N7001T for unidirectional level translation.

    If there are multiple bits in your application, let me know and we can suggest other devices suitable for you.