Other Parts Discussed in Thread: SN74AUC244
Hello,
We are planning to use the SN74AVC2T244 as a converter from either 3.3V or 1.8V to 1.35V. The part is expected to drive 8 loads (2 mA per load).
According to the datasheet, Vout_low max is 0.35V low at 1.4V rail and 2mA load. Is there a way to extrapolate / predict Vout_low max at 1.35V and 16 mA load ?
Same question for the Vout_high min.
Alex